AXIS#.DBILIMITACTUAL
Description
This parameter returns the minimum value of the following parameters: AXIS#.DBILIMIT , AXIS#.ICONT , AXIS#.MOTOR.ICONT .
Example
Assume AXIS1.ICONT = 3 Arms, AXIS1.DBILIMIT = 1 Arms, and AXIS1.MOTOR.ICONT = 2 Arms. Then AXIS#.DBILIMITACTUAL will return 1 Arms.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-07-00-000 |
General Information
Type |
Read only |
Description |
Returns the minimum value of the AXIS#.DBILIMIT , AXIS#.ICONT , AXIS#.MOTOR.ICONT keywords. |
Units |
Arms |
Data Type |
Float |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
Fieldbus A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.DBILIMITACTUAL | 0x5000 | 0x11 | UDINT | 1000:1 | - | RO | False |
AXIS2.DBILIMITACTUAL | 0x5100 | 0x11 | UDINT | 1000:1 | - | RO | False |